WHEN.PLCMD

Description

Records the value of PL.CMD when the when-condition is satisfied. The when-condition is checked once per 250 microseconds.

General Information

Type

R/O

Units

Position units

Range

N/A

Default Value

N/A

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1174

Yes 64 bit No

M_01-05-11-000

Related Topics

PL.CMD | When